Other Parts Discussed in Thread: TPS54540
用TPS54540做了一块板,具体参数:Vin=DC36v Vout=15v Iomax=2.5A,F=500K,其他参数按照官网设计工具计算得来。现测得在ta=26℃时,用热电偶测得IC表面(塑封顶部正中心位置)温度73℃,IC功耗计算PD=826mW。IC热阻值
问题:1.按照规格书提供热阻值,计算方法1:θJCtop=45.8℃/W时 TJ=Tc+PD*θJC=73℃+0.826W*45.8=111.83℃/W ;计算方式2: θJA=42℃/w TJ=Ta+θJA*PD=26℃+0.826w*42℃/w=60.7℃。两者相差太大,方式2中结温60.7℃小于方式1中表面温度73℃,这个就很难理解,如果2式成立,理论方式1中表面温度应该低于60.7才对啊(TA=30℃下,TI官网设计工具得出的结温51.47℃
)。是不是我计算方法问题,还是测试点问题?如有问题,请告知正确的计算方式?2.ψJT含义? 还请TI大牛指导,谢谢!