Other Parts Discussed in Thread: XTR111
各位大神好,我在使用XTR111使用如下电路图时,
因为需要给后级放大器提供电压,所以在电流输出环上增加27V稳压管,现在发现XTR111使用32V供电时发热很严重,XTR111工作电压小于32V时观察输出不正常,请问XTR111正常温升为多少?像上面使用的话为了能使电流环上电压达到27V(稳压管为27V),XTR111的供电电压应该为多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: XTR111
各位大神好,我在使用XTR111使用如下电路图时,
因为需要给后级放大器提供电压,所以在电流输出环上增加27V稳压管,现在发现XTR111使用32V供电时发热很严重,XTR111工作电压小于32V时观察输出不正常,请问XTR111正常温升为多少?像上面使用的话为了能使电流环上电压达到27V(稳压管为27V),XTR111的供电电压应该为多少?
Hi
最好供电可到44V,所以32V供电没有问题。
建议你确认一下MOS的选择,可以参照datasheet的型号或者说明。
这个芯片最多25mA左右的电流,如果Vsp与IS压差很大,是会导致发热的,因为这个时候功耗是很大的(你可以将当做是LDO来评估功耗)
( 或者你找放大器板块的工程师再确认一下,而这里是电源板块)