This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请教一下,BQ40Z50-R1,现在cycle counts= 2,UPDATE STATUS = 0X0E,
但是Gas Gauging 项目下面的
Max Error项的
Time Cycle Equivalent = 24h,
Cycle Delta = 0.05% 这样对吗?
Condition Flag项的
Max Error Limit = 100%,这是正常还是不正常?