论坛的大虾,在测试时出现,在空载和加载的情况下,24V输入时,输出无电压输出。将输入电压逐步减小到12V左右时,电源就输出正常。工作一段时间后,断掉输入,再次上电,输出正常。长时间断电后,第一次加电,没有输出。此时LM3481 DR输出为间断的控制信号。不知道是哪方面影响到的。5125.snvu528评估板.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
论坛的大虾,在测试时出现,在空载和加载的情况下,24V输入时,输出无电压输出。将输入电压逐步减小到12V左右时,电源就输出正常。工作一段时间后,断掉输入,再次上电,输出正常。长时间断电后,第一次加电,没有输出。此时LM3481 DR输出为间断的控制信号。不知道是哪方面影响到的。5125.snvu528评估板.pdf
HI
在高压24V输入时,无论是加载还是空载都没有输出,只有将输入降低到12V时才能正常启动吗?
将电路图传上来看一下,最好还有看一下Layout.
Hi
只是40V供电,不需要这部分电路。(这部分电路设计上应该是有问题的,即便供电超过48V,也不建议采用这个电路)
芯片供电脚上的电路稍微大一点。
陶工:你好!
刚才测试了,换了一个LM3481后,在40V输入下,空载及加载都能正常启动。估计是在之前的测试中将LM3481这颗芯片搞不良了,就出现莫名其妙的一些问题。另外你提出过压保护那块电路有问题,我该怎样调整。