电路图如下图所示:
功能描述:POWER是用USB的5V供电,在正常状态下GPIO0是周期性的由低变高,控制Q7周期性的通断。在实际测量时,用示波器测量R26两端的电压,R26靠近Q7一端的电压是正常的跌落,但是R26靠近POWER一端的电压也跟着跌落了,跌落的电压有2V左右,示波器抓到的图形如下:
其中红色的图是靠近Q7的D极的电压,蓝色是POWER的电压,请教各位大神这是怎么回事???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
Q7不导通(GPIO高)的时间, POWER 通过R26,R28给Q6/Q5 G极充电,所以R26上是有电流的,并且导致短暂的压降。
POWER 这里应该有个电容稳压的,靠近R26附近。
Hi
你测试的不是Power 的电压,而是Q7在关闭时的电压,如果R26上因为给两个MOS G极充电有电流,你实际测量的电压就是POWER减去R26压降。
如果其他板子是正常的,代表R26上电流不对,交互验证一下是否是MOS由问题,因为电阻不会消耗电流,MOS有可能。(我觉得这个波形是正常的,没有什么问题)
Hi
我一开始时看着是Power的电压,看着看着就看成Q7 D极的电压了,因为这样就合理了。
Power 这里没有稳压电容,输入电压是有可能拉低的。建议你比较一下layout或者加电容看看。