我用3.3V给用INA214的V+供电,0.1Ω作为分压的电阻,高端检测,分压电阻在VCC和负载中间,VCC为6V,但是在输出端没有任何输出,请教一下,这是什么情况,我是要吧V+也接到VCC一样的6V上么,还是接3.3V就可以。
我的最大的电流为0.2A,平时的电流为0.02A,做电机的电流检测。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
V+接3.3V就可以了。
REF怎么接的?另外IN+和IN-怎么接的?
输出端没有任何输出是如何测量的?
从电路图上看IN+和IN-接反了。电流应该是从VCC60流向VM引脚。
不确定是不是这个问题。REF接地,此时检测到的电流应该是负方向,输出电压为负,箝位到地。
另外输入电阻后端,建议加差分电容滤波。