Other Parts Discussed in Thread: TPS61070
需要找一款3.5V输入,5V输出的升压芯片,输出电流500mA,初步选型为TPS61070,但是在读datasheet时,发现这款芯片3.3V输入时,只能输出150mA电流,请问这是怎么计算的?数据手册中Switch current limit=600mA,请问这个参数与输出电流什么关系?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
首先,根据规格书3.3V输入5V输出,负载电流应该在300mA.
其次,升压芯片的限流等效输入电流的峰值电流,不等效输出电流的平均电流。
简单计算:
Pin = Vin x Iin
Pout = Vout x Iout
Vin<Vout 假设效率80%,可以通过输出功率计算出输入电流的平均值。
换算之后,输入电流是肯定会大于输出电流的,所以输入电流再加上20%~30%的纹波电流等于限流值。
用这个方法可以简单估算负载电流最大值。
谢谢。
去这里找一个吧
https://webench.ti.com/webench5/power/webench5.cgi?origin=ti_panel&lang_chosen=en_US&VinMin=3.3&VinMax=3.4&O1V=5&O1I=0.5&op_TA=30