我用LM22676_ADJ 芯片,将12V 转成5V ,要求输出电流是3A,根据datasheet中电感计算公式,公式12,应该是68uH,但是用webench 软件设计出来是12 uH,,为什么会有这么大的差异?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用LM22676_ADJ 芯片,将12V 转成5V ,要求输出电流是3A,根据datasheet中电感计算公式,公式12,应该是68uH,但是用webench 软件设计出来是12 uH,,为什么会有这么大的差异?
Hi
其实主要的重点在于电感饱和电流,建议大于最大输出电流的1.2倍。
在计算感值时,纹波电流取值20~40%的满载输出电流。datasheet和Webench的取值上可能存在差异。