This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54160A

Other Parts Discussed in Thread: TPS54160A, TPS54361, TPS54360, TPS54560, TPS54561, TPS54160

TPS54160A芯片介绍上说最小输入电压是3.5V,可是在我测试过程中,低于6V的输入对应的3.3V的输出就开始不稳定了,我下载了EVM测试板的资料,上面写该芯片推荐的工作电压范围是6V-60V,我想问是不是低于6V的输入,这款芯片就不太支持了?如果不是,为什么5V左右的输入电压对应的3.3V输出跌落的很厉害?

  • Ying

    你好,可否用示波器观察当输入电压低于6V时占空比是否减小,随着输入电压减小,占空比是否减小加剧?

  • Bootstrap Voltage (BOOT)

    The TPS54160A has an integrated boot regulator and requires a small ceramic capacitor between the BOOT and

    PH pin to provide the gate drive voltage for the high side MOSFET. The value of the ceramic capacitor should be

    0.1 μF. A ceramic capacitor with an X7R or X5R grade dielectric is recommended because of the stable

    characteristics over temperature and voltage. To improve drop out, the TPS54160A is designed to operate at

    100% duty cycle as long as the BOOT to PH pin voltage is greater than 2.1 V. When the voltage from BOOT to

    PH drops below 2.1 V, the high side MOSFET is turned off using an UVLO circuit allowing for the low side diode

    to conduct which allows refreshing of the BOOT capacitor. Since the supply current sourced from the BOOT

    capacitor is low, the high side MOSFET can remain on for more switching cycles than it refreshes, thus, the

    effective duty cycle limitation that is attributed to the boot regulator system is high.

    这个是说当boot与PH之间的电压低于2.1V时,本周期占空比会被chop,是否可以增大0.1uF的电容?测试效果

  • 产生这种现象的原因正如Max Han描述的。 输入输出电压压差较小,54160在空载和轻载时的输出会不稳定。如果增加负载则54160的输出会恢复稳定。解决方案:

    1)如果最大输入电压小于8V,可以用一个齐纳二极管从输入电压Vin连接到芯片Boot脚。这样输入电压降至4.3V左右任然可以保证空载输出电压稳定。

    2)如果最大输入电压大于8V,推荐用齐纳二极管从输出电压连接到芯片Boot脚。这样也可以改善稳定性。不过效果不如(1)

    如果能知道您的详细电源规格和要求,我们能给出更合适的方案。

  • Jerry hi,

    我现在用TPS54160A设计5V转3.3V时,也遇到了上述问题。正常5V输出3.3V没问题。但我这个项目有输入5V拉偏10%的要求,在轻载时输入4.5V或4.6V时,3.3V输出为2V左右,启动时在3.3V后端加上负载,3.3V输出正常,但我的系统刚启动肯定是轻载。

    我想咨询下,这颗芯片是否已经验证过就是您说的上述问题,齐纳二极管的使用方式及选型如何考虑,这样设计的原理是什么。

    另外是否有pin to pin兼容的不存在上述问题的可替代芯片,tks!

  • Hi

       能够帮忙发成为新贴,谢谢。

  • 你好,由于这是异步电源,所以会存在这样的问题,但是有些异步电源芯片内部存在一个MOS专门用来为BOOT充电。这种芯片可以避免这样的问题, 如TPS54360和TPS54361,TPS54560,TPS54561。

    或者你可以直接采用同步电源(外部不用加肖特基二极管的),可以利用WEBENCH搜索符合你要求的芯片,Pin-to-Pin 的貌似没有

    关于二极管的选取,只要导通压降尽量小的就可以

  • 具体原理参考附件。楼上说的是对的。

    附件是专门针对TPS54160系列产品该类问题的解决方案。

    Methods to Improve Low Dropout Operation.pdf
  • 感谢快速详细释疑,非常有帮助!

  • 如果问题已经,请点击下角,“这问题已被解答”。这样也方便其他工程师参考。谢谢!