我这边需要给一个电阻提供2个方向的连续电流,所以只能采用H桥模式搭建电路。但是我只能提供20V 400uA。我想问一下 这个L393芯片可以使用吗 如果不行,能不能各位大佬提供一款可供我使用的H桥芯片啊 谢谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我这边需要给一个电阻提供2个方向的连续电流,所以只能采用H桥模式搭建电路。但是我只能提供20V 400uA。我想问一下 这个L393芯片可以使用吗 如果不行,能不能各位大佬提供一款可供我使用的H桥芯片啊 谢谢!!!
我从耳机口输出的电源,经过恒流源固定输出400uA的电流了,电压范围大概15V到25V左右吧。 我之前一直使用ZXM61N03和ZXM61P03搭建H桥 一直被击穿 也不知道是什么情况。。