问题如下:
我打算使用LM2588-ADJ,输入12V,输出±12V给板子上的1个AD8276+4个OPA211+1个THS4131供电,自制的变压器输出电流能力可达300ma,电路如下。
我想问问用这种flybuck的方式给一些放大器(如OPA211)供电会不会给芯片带来不好的影响。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
对于AD,或者运放,建议在其输出增加一级LC,甚至高PSRR低noise的LDO.
你好请问LC的值怎么选?
在输出级和放大器电源引脚都放置旁路电容行不行
有合适的LDO推荐吗,输入12V输出正负12V或者输出正负15V
对芯片影响不大,主要是噪声对后级的干扰,对于LC滤波器,设置截止频率低一点就可以,建议LDO可以看看TPS7A39