This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果 我改用TPS7A4701和TPS7A33实现输出正负15V,输出电流达到300ma即可,您觉得有必要将正负24V再经过DCDC变换到比如正负18V吗
HI
压差9V,300mA,功耗是2.7W, 选择TO220封装Junction-to-ambient都没问题的, 但是芯片温度会很高。(或者热阻比较小的焊接方式)
不过建议你用DC/DC,损耗小,效率高,芯片温度不会很高。
这主要是功耗体积与成本的权衡了,如果不考虑功耗,是没有必要的
如果你布局很紧凑的话,不建议用LDO,
或者可以考虑用BUCK-BOOST进行24V转正负15(如果对PSRR要求不高)http://www.ti.com/lit/an/slua838/slua838.pdf