我设计了一个非隔离POE模块,采用PD芯片TPS2378,和DCDC TPS54360,带载3.5A,但是实际调试带载2A,TPS54360就会损坏,而且SS56 SMB也会短路。用示波器测试SW电压,最高才50V,求教大神给点分析建议。下面是TPS54360的原理图,PCB板是两层板,带载1.5A时,电感的温度为66℃左右(常温)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
肖特基续流二极管电流肯定没有问题,只能是电压。POE供电时最高电压是57V, 如果是这样的话建议选择80V或者100V的肖特基二极管。
即便是稳定的50V,如果SW脚layout不好,是可能有一定的spike, 能否将波形穿上来看一下?
首先对于开关电源,最好是4层板,其次Layout也很重要。
1,SS56短路你是怎么测量的?是在板子上直接测量还是拿下来测量的。如果是在板子上测量那就也有可能是SW击穿,直接短路到GND。若是SW击穿,则应该是SW节点的振铃太高,所以你最好是更改Layout,其次在boot加电阻(10ohm以内)或snubber电路。若二极管短路,则根据SW节点的振铃峰值来选取合适耐压的二极管。
2,输入电压48V,如果你输入引线较长就容易形成LC谐振导致Vin超过65V,也会造成芯片损坏,方法:加220uF的电解电容。加稳压管
我们这边示波器带壳200M的,我测过SW的波形,显示峰峰值最大才50.8V。我今天换一个SS510验证下。
你好,我这边在板子上和拆下来都量了是导通的,我换个SS510时试试。
2A不稳,说明环路不稳定,建议你用WEBENCH重新优化参数。
还有你两层板且两面都有电路,很容易造成串扰的,建议你用现成两块板一块只用buck一块只用2378,串起来看看是否能稳定工作
我单独测了下TPS54360可以稳定输出3A,现在把2378和54360用两块板子连在一起,挂2A负载会好很多,但是偶尔电压还是会跳动一下。
那基本可以定位是布局问题,建议重新布局,4层板,两个芯片在同一平面。具体器件摆放可以参考数据手册或者WEBENCH
你有C8大电解电容,问题不大,注意,一定要四层板,
您好,我这边四层板调试,现在比较稳定,测试效率在1A 88.8%,2A 87%,调试了下RT/CLK脚的电阻,改变阻值180Kohm~240Kohm,频率改变了但是效率没有变化多少,对于54360有没有一些地方可以来提高效率的地方。
你的频率变化范围太小了,当然看不出来
你改到100KHz就可以看出来了,当然频率变化,电路的其他参数也要随之改变,具体取值可以参考WEBENCH
对于效率,要选压降尽可能小的二极管,电感电容的寄生电阻也要尽可能小
是的,超过max电压会击穿芯片的,你可以在SW节点加入snubber电路(串联R=2ohm,C=2000pF到地)或者在boot电容上串一个10ohm左右电阻