Other Parts Discussed in Thread: LM2664, TPS62175, TPS63710, TPS63700, TPS5430, TINA-TI, LMR16020, LM2663, TPS62173
hello,
如题,后端接两个正负5V电压的运放,电流在100mA以内。
看了一下TI选型,发现有款LM2664,是+5V输入,-5V输出,但是手册上没有看到-5V输出时的电流曲线,
请问在保证-5V输出的时候,电流是不是就达不到40mA了?
我现在用其他两款+5V转-5V的芯片,发现一款芯片虽然标称-5V输出,但是实际上只有一半,-2.5左右。
另外一款是-5V输出,但是接到其中一个芯片上,会导致+-5V短路。我加了电阻做负载,发现在-5V输出时是达不到标称的最大电流的,
会把电压拉低。
不知道TI的LM2664是否有这样现象,还是说这种现象对于电荷泵来说,是正常的?
或是有没有其他可以推荐的芯片?如果用12V转+-5V的芯片,感觉电路都太复杂,想用12V转+5V,+5V转-5V的设计。
之前推荐的像TPS54560,看手册输入电压要在18V以上,不知道是不是这样?