4节1.5v电池串联满电7.2v@3000mA作为设备电源,4节1.5v电池串联在4.8v时定义为缺电;
LMR62014DCDC 输出5v驱动步进电机;
步进电机的工作电源范围是3.6v-24v;
TPS62742DCDC输出3.0v为stm32l073r、cc2541、spi_flash和NXP_NFC供电;
设备工作模式有:睡眠、唤醒、工作这3种模式
请问:
作为低功耗产品,选用这2个LMR62014、TPS62742是否合适?
是否有更优秀的芯片组合?
感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
4节1.5v电池串联满电7.2v@3000mA作为设备电源,4节1.5v电池串联在4.8v时定义为缺电;
LMR62014DCDC 输出5v驱动步进电机;
步进电机的工作电源范围是3.6v-24v;
TPS62742DCDC输出3.0v为stm32l073r、cc2541、spi_flash和NXP_NFC供电;
设备工作模式有:睡眠、唤醒、工作这3种模式
请问:
作为低功耗产品,选用这2个LMR62014、TPS62742是否合适?
是否有更优秀的芯片组合?
感谢!
Hi
TPS62742是低功耗超低静态电流的降压芯片是可以的。
LMR62014是升压芯片,你的输入是4.8~7.2V, 输出做5V,是要这样吗?可以做,但是我想找一下是否有更合适的芯片,你确认是要做5V输出吗?
HI
如之前所谈,选择升降压芯片,可以选择TPS63061: http://www.ti.com.cn/cn/lit/ds/symlink/tps63060.pdf