采用两片EMB1428进行电池均衡,电池为12节磷酸铁锂电池,每片芯片负责6节电池,EMB1428部分参考电路依据TI官方参考设计,详情 www.ti.com.cn/.../TIDA-00239 其他部分将1499替换为3A 最大电压4.5V的功率模块,只对低电压电池进行充电处理,EN、DIR、DIRRT DONE引脚用单片机模拟出对应的时序信号。现在已经分别测得emb1428部分已经正常工作,返回值以及对每路电池通道开关均正常。同时功率模块也能正常工作,但是两者结合之后,很容易出现1428芯片坏掉的问题,具体表现在45引脚VDDP与地之间短路,返回值为1011(b),请问这种情况可能是哪里出现了问题,怎么解决?