Other Parts Discussed in Thread: TL431, TLV431A, TPS57040-Q1, TPS797
hi:
1、如图中, tl431的工作时的电流应该是大于1ma的?
2、TLV431A -Q1,是否代表典型电流为80 uA?
- Low Operational Cathode Current, 80 µA Typ
如果不是,能否推荐低电流的型号,5V基准电压芯片,使用TPS57040-Q1,12V/5V 。
谢谢!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TL431, TLV431A, TPS57040-Q1, TPS797
hi:
1、如图中, tl431的工作时的电流应该是大于1ma的?
2、TLV431A -Q1,是否代表典型电流为80 uA?
HI
你所要是5V的供电电压还是要5V的基准电压?
如果是供电,供电电流需求是多少? 如果是基准电压,基准精度要求是多少?
从你的意思看是否是要芯片本身的内消耗尽量小,一般LDO精度是2%, 消耗都可以是就1uA左右,例如TPS797.
如果是供电,要看输入电压,输出电流,选择一些超低静态电流的芯片。