This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2407xt-技术咨询

Other Parts Discussed in Thread: BQ24075T, BQ24072T

请问:

1:关于下图参数,是针对VIN有输入的情况吧?比如VIN是6V,BQ24075T的VOUT输出是5.4V到5.6V,是不是可以理解,5V输入的时候,BQ24075T的VOUT输出最大是4.5V,BQ24072T的VOUT输出最大是Vbat+225mV,

2:如果没有VIN输入,Vout是跟随battery的电压的,比battery稍低,

现在电池的标称电压是3.8V,最大充电电压是4.35V,请问选哪一款更合适,谢谢,