ucc21520在全桥应用中,VDDA和VDDB可否用同一电源供电,一次侧供电电压3.3V 与18V是否有区别
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. VDDA和VDDB可以使用同一电源供电,但是一般不会这么做。UCC21520一般都是用在高压隔离环境,所以VSSA和VSSB的电平是不一样的,VDDA和VDDB分别参考VSSA和VSSB,所以不用使用同一路电源共地。如果你说的是自举电路的同一路电源,二极管实现隔离。那么是可以的。
2. 一次侧3.3V和18V,只要高于UVLO 电压2.7V,那么原则上没区别。主要注意是INA和INB引脚的输入电压不能高于VCCI的供电电压。如果VCCI更高,那么INA/INAB的输入电压范围可以更宽。
Hi
2个驱动的电压能够用一个,看两个驱动的GND.