This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54560电路webench显示Design cannot be created with this device. Please press OK and select a different device from the list

Other Parts Discussed in Thread: TPS54560, LM5175

您好,我看到TPS54560可以为降压开关电源芯片,可以输出12V5A,所以想做一个输入10-35V,输出12V5A的电源模块,但是在使用WEBENCH设计的时候出现Design cannot be created with this device.  Please press OK and select a different device from the list Or click below to show why parts were not found。应该是不能使用TPS54560实现此电源模块,因此我了解以下几个问题:

(1)TPS54560可否实现此模块

(2)如何使用WEBENCH设计TPS54560电路图和PCB

(3)若可以使用TPS54560,那么需要注意哪些地方

  • 参照slvu863进行了TPS54560的设计,将R5更换为143Kohm,启动电压设置为9.5V,停止电压8V,根据IHYS = 3.4μA,VENA = 1.2 V,I1 = 1.2μA。计算R1 = 442Kohm,R2 = 60Kohm,我想了解以下几点:

    (1)看到其它帖子有设计电路后进行仿真的,不知道如何仿真我修改后的电路;

    (2)如果不可以仿真,那么我设计的电路原理是否正确

    (3)看到后面的物料清单电容要求比较高,那么哪些物料是必须严格要求的,是否有替换

  • 这是降压芯片,你输入比输出低是不可能实现的,除非有升降压芯片,如LM5175

  • HI 

        你可以借助Webench选型,在设计。

        TPS54560是降压芯片,如果你要用这款芯片,输入必须大于输出一定电压。