Bq24610冲六串锂电池,电池电压设置25.2V 输入电压26.2V 充电电流1.5A 截止电流0.15A,电感6.8uH 电容20uF
电池充电电流降到1.3A时,能听见明显的电感嘶嘶声,而且开关节点PWM频率由正常时620K下降到300K左右。请问有人遇到过没?
再有,同样一块电路,设置给三串锂电池充电时整个周期很正常,未发现此故障。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
有没有确认电感质量问题。
如果电感没有问题,你需要确认一下电路的稳定性(可以测试sense电阻波形,或者驱动)
Hi
可能和芯片驱动能力有关,也可能和驱动的供电有关,建议你排查。
SiS412DN的Qg远远小于FDS4470, 即便你选择40V的管子,也建议你选择尽量小Qg的40V管子。