This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

路径管理方案邀请!

Other Parts Discussed in Thread: BQ24610

Hi~

    贵司的 BQ24610芯片是 电池组优先输出供电的,但没有电池的情况下才切换到外部电源(适配器)供电。

    但我们需要的产品刚好相反,是外部电源(适配器)供电为优先输出,当在没有适配器的情况下才切换到由电池组供电。

     想问一下有没有这样的芯片 或者方案也可以?

     参数: 电池组的电压是12.6V(3个18650电芯串联),输出的电流是2A以下。

                  电源切换时要求无缝切换。 

      谢谢! 

  • Hi

        这类芯片都是在电池和适配器同时存在的情况下,是优先适配器供电的,datasheet可能没有表述清楚。

        

  • datasheet 表述清楚了,默认的是电池组供电,当没有电池时才由适配器供电。

    The bq2461x automatically switches adapter or battery power to the system load. The battery is connected to the
    system by default during power up or during SLEEP mode. The battery is disconnected from the system and
    then the adapter is connected to the system 30 ms after exiting SLEEP. An automatic break-before-make logic
    prevents shoot-through currents when the selectors switch.

     实际使用BQ24610 这款IC测试也是这个结论,电池组默认供电。

     我只想找一款 默认是适配器供电的芯片IC, 当没有适配器才由电池组供电。 

     谢谢!