我看文档说J2连接器部件号为43025-1600,配对连接器的压接针是零件号46235-5001(或46235-5002),上淘宝搜了下都是一个一个的,如下图
想问下有没有做成一整个的对应J2的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
直接找代理商买: (黑体字)
The mating connector from Molex Connector Corporation is part number 43025-1600.
Digikey Corporation: WM2490-ND. The crimp pin for this mating connector from Molex Connector Corporation is part number 46235-5001 (or 46235-5002). Digikey Corporation: WM2258TR-ND or WM2258CT-ND. (An alternate base number for different plating option is WM2259.)
The part number for the crimper to create custom cables using the above parts from Molex Connector Corporation is: 63819-2900. Digikey Corporation: WM4747-ND.