请大师给些建议,如何实现大功率,本人是菜鸟,最大做过300W,十分期待您的答复!并非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
不需要隔离,可以用C2000之类的数字芯片做多相降压控制。
隔离可以用UCC28950全桥移相来做,或可以用2个芯片并联来实现较大功率,如5000w。
UCC28950,TI有提供1600W的方案:
http://www.ti.com.cn/tool/cn/pmp6712 (如果96V输入,或可根据这个电路来改)
谢谢您的指点,好的,那我今天要的答案有回应了,明天根据网址下载资料.因考虑后面的方便,肯定会有疑难问题的,若方便的话,请留下电话,或发邮件给我,chenyuerhao@163.com,非常感谢!