This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

±220V输出隔离型电源模块设计



大家好,公司最近有个项目,时间挺敢的,老板要求一次搞定,具体技术参数如下:

1. 输入电压: DC9V-DC18V;

2. 输出电压:±220V输出,负载电流30mA;(特别说明,模块正常工作时,±220V只有一组输出带带载,既±220V不同时工作);

3. 输出电压调整率≤2%,输出纹波≤1%;

4.转换效率≥65%;

5.电源架构:单端反激隔离型,隔离电压1000V;

6.工作温度:-40℃-50℃;

7. 变压器选用EPC贴片变压器。

请问大家有没有相关的设计方案,先谢谢大家了!