This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我们现在有个需求,15V升压至75V,功率5W左右,不隔离就可以,请问TI有什么简单的方案吗?直接电感BOOST升压可以吗?有什么控制器推荐?
Hi
用外部MOS的升压芯片都可以做,例如TPS40210,lm3481/78
内置MOS则需要借助耦合电感,因为大部分芯片SW脚耐压都是小于75V的,设计可以参照:
TPS61040输入电压偏低,并且开关电流偏小。 如果15V输入可以选择TPS61170. 设计架构如上。