Other Parts Discussed in Thread: TIDA-00689, UC3844, LM5022, LM5160, LM2587
24V输入,隔离输出3组电压,第一组5V,1A;第二组﹢15V,200mA,第三组-15V,200mA;5V与±15V需要隔离。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TIDA-00689, UC3844, LM5022, LM5160, LM2587
24V输入,隔离输出3组电压,第一组5V,1A;第二组﹢15V,200mA,第三组-15V,200mA;5V与±15V需要隔离。
Hi
底下那个文档: http://www.ti.com.cn/cn/lit/an/snva005b/snva005b.pdf
就是用来做完全隔离的。
下面的文档是指出了副边与原边输入完全隔离,但是我的意思是±15的地和5V的地没有隔离。
可以邮件huangmin@scaeme.cn TEL:15884484844 交流
如果有变压器设计能力,可以用flyback绕多组副边出+5V,+15V,-15V,控制器如UC3844,LM5022,LM5160
我主要是想找个简单方便的解决问题。如果有现场的变压器,就直接采用
请问参考这个文档。12V隔离输出5V2A 变压的规格是怎样的?
看文档的图纸。 LP 22uH N1 1? N1 是多少uH 匝数比 是多少呢?
有没有详细规格。或者变压器型号推荐。谢谢!
你可以参考这个文档来设计你的变压器。原理都差不多