This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

急!!!BQ34Z100配置实用

Other Parts Discussed in Thread: BQ34Z100

环境说明:电池是LiFePO4,16节电池串联,容量为20Ah,电压范围在48~58.4,配置的跟踪电阻为2.5毫欧,实用IIC通信

配置:由于BQ34Z100实用为1~14节,所以配置为14块,然后电池配置的充电电压和截至电压都是16块的电压,却配置为14块的形式。

问题:在测试中,发现电量的变化有跳变,昨晚测试放电,充满为95%,开始放电,以2.5A电流放电,一个小时左右后,读取的剩余电量有91%突然下降到31%,请问下这个跳变是什么引起的,并且在放电中一个小时的电量变化应该为10%左右。为弄明白电量的突变是什么引起的,还是有参数没有配置正确。