Other Parts Discussed in Thread: TPS61165
准备用TPS61165做LED屏幕的背光驱动芯片,还需要一个VGH、VGL电压发生电路也想用TPS61165做,但是看了数据手册,没有做恒定电压输出的资料,不知道是否可以像RT9293芯片一样通过分压电阻做固定电压输出?有没有推荐电路啊VGH 16V左右,VGL -7V左右?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
增加47kohm, 主要是担心PWM信号没有的情况,这样等同CTRL悬空。
输出电容确实不需要这么大,建议是1uF~4.7uF。