This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

移相全桥驱动震荡问题求助



最近用DSP28035做一款移相全桥的可调电源,遇到了驱动震荡的问题,具体如下,请大神出出主意,非常感谢!

电源参数是:输入电压直流310V,输出电压100V,50A(0-100V可调)

开关频率:100KHz

MOS管型号:IXFH80N65X2

原边钳位二极管(D5和D6)型号:DSEI60-12A;

原边谐振电感:铁氧体ETD49,开气息之后,4uH;

主变压器:铁氧体EE85    匝比6:3:3(不开气息,原边电感量355uH,漏感2.5uH)

副边二极管:MUR3060PT(三只并)。

输出滤波电感:铁硅铝磁环,12uH。

输出滤波电容:220Uf/250v  五只并联。

驱动波形在没有开功率电之前是好的,加了功率电之后驱动有震荡,输出电压越低,震荡越厉害,负载约轻,震荡越厉害。