This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

400W抗电压跌落、浪涌电源(符合GJB 298)



400W抗电压浪涌跌落抑制器

产品要求:

1、 正常输入18Vdc36Vdc,直通输出,最大功率400W。

2、 输入跌落电压最低6V/1秒(GJB 298),输出功率160W,输出电压17V

3、 输入过压最高 100V/500mSGJB 298),最大电流10.8A,输出电压37V

4、 工作环境温度:-4085℃。

5、 体积尽量小,可协商。

6、 成熟产品优先,前期要6只左右样品,进行整机验证,后期每年会有批量生产 。

联系电话:13811077085