各位TI的专家与大神们:
我的电池主板使用的是BQ4050电源管理芯片,学习成功后MaxError为2%(learned fcc =5100),但是用着用着到后面出现了MaxError到了11%(learned fcc =32763),这个是怎么回事呢?是哪里的参数引起了他的变化呢?急等。
感谢感谢!~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位TI的专家与大神们:
我的电池主板使用的是BQ4050电源管理芯片,学习成功后MaxError为2%(learned fcc =5100),但是用着用着到后面出现了MaxError到了11%(learned fcc =32763),这个是怎么回事呢?是哪里的参数引起了他的变化呢?急等。
感谢感谢!~
maxerror
Max error is incremented internally by 0.05% for every increment of CylceCount after the last QMAX update. MaxError is incremented in the display by 1% for each increment of CycleCount.
Event MaxError
Setting Full reset Set to 100%
QMAX and Ra table update Set to 1%
QMAX update Set to 3%
Ra table update Set to 5%