Other Parts Discussed in Thread: TPS54620, TPS5450
希望TPS5450实现24V转12V,原理图的后端有两个2级DCDC芯片TPS54620和LTC3633,分别用12V转3.3/3.3/5V,
贴回来两块样板,发现TPS5450的输出异常,一块是7.2V,一块是2.6V,两块板子对应的Vsense分别是0.72V和0.26V,是输出电压的1/10。
按照手册上Vsense引脚应该是稳定的1.221V才正常,
我将2.6V输出的板子拆掉输出端电感之后,发现芯片的1脚和8脚电压都是0,然后我把一个以前用5450做的24V-5V的板子电感拆掉,1脚是28V,8脚是22V
由于这个芯片用过很多次了,都没出过问题,所以这次设计的时候没有在12V的输出端加磁珠与后级进行隔离,无法断开进行测量。
想请教各位,接下来怎么定位问题