最近在做BQ24610充电器电路板,可是充电异常,黄色的是hidrv,蓝色的是lodrv信号,原理图参考的是datasheet中的typical application。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近在做BQ24610充电器电路板,可是充电异常,黄色的是hidrv,蓝色的是lodrv信号,原理图参考的是datasheet中的typical application。
Hi
你测试的时候输入电压以及电池电压分别是多少?输入电压测量点取自Q17输入端。
Hi
19V是使用示波器测试高边MOS输入端?
测试此时的充电电流是否小于你设置的电流? 还有做其他测试?
对,高边MOS 输入端的电压, 测试还发现充电电流小于我设置的电流,并且充一个小时左右STAT1和stat2 都无效了;
Hi
前端两个MOS导通, 测试VCC,REF电压正常,此时TS电压多少? 然后确认一下输入源是否限流? 以及输入前端的sense电阻信号是否过流(包括侦测电阻损坏)?
最后确认一下是否是充电电流过小(sense电阻电压小于1.25mV, 见datasheet 19页:9.3.12 Cycle-by-Cycle Charge Undercurrent Protection)
VCC 和vref这两个电压都正常,TS电压是1.69,在充的时候SRN 采样电阻两端的压差是30MV,我目前还遇到一个问题就是充一会后,stat1和stat2两个就都OFF了
我现在换了另一块电路板,刚开始充电正常,电池充满后对电池进行放点,再次充电的时候发现一直以160MA左右的电流充电,stat1有效,stat2无效,充一个小时左右后,stat1无效,stat2无效;