Other Parts Discussed in Thread: UCC27323
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
这个驱动器芯片,用于增加一些PWM控制芯片的驱动能力,本身并不会产生PWM信号,而是由主控芯片输出的PWM芯片给到INA/B, 而得到一个强大的PWM1/2驱动信号,可以用于驱动更大Qg的MOS(或加快上升速度),以及驱动IGBT.
你好,能讲解一下sink 与source电流测试原理吗,看不懂如何测试的
按照上面那个电路图是可以产生双路PWM的、芯片是使用MC33151、我买回来UCC27323装上去也是有PWM波的、但是我不知道产生PWM的原理
你好,
PWM信号是由前级产生输出给芯片的,芯片本身并不产生PWM信号。UCC27323只是栅驱动器,用来增强栅驱动信号的能力。
希望可以帮助到你,谢谢。
你好,
你可以看一下INA和INB左边信号接的是什么,一般来说是前级电路给出的两路栅驱动信号,然后再经过UCC27323加强驱动能力。至于在芯片输入和输出间跨接的串联RC电路,应该是用来抑制驱动信号上的振荡。这是因为如果走线比较长,走线上的寄生电感在输出信号的上升下降沿处,会和栅极电容一起振荡。后加的RC一端接一路输出,另一端接相应输出相反的那路输入,推测这两路信号是互补的,那在某一路信号上升沿时,另一路为低,振荡可以RC网络被滤掉。如果PCB布局较好,栅驱动走线很短,同时工作频率不高,这个RC是可以省掉的。
希望可以帮助到你,谢谢。