This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lm3478掉电压的问题

Other Parts Discussed in Thread: LM3478

大家好,我是第一次做开关电源,选用lm3478电源芯片,dc-dc变换器,输入电压12伏输出电压24伏,最大输出电流1.5安,在调试中,只有当所带负载电阻达到1000ohm及以上电压保持稳定,在负载电阻低于1000Ohm时,电压掉得厉害,比如带100ohm电压由稳定的24伏变成10伏,我把Isense引脚接地就变成13伏,我把改调的调了,不知哪里有问题?请教大侠们了,给我指点一下

  • Hi

        对于无法带载,你需要注意如下问题:

        1.  你需要选择饱和电流足够的功率电感,推荐大于最大输入电流的1.3倍。   最大输入电流是最大输出电流*输出电压/效率85%/最小输入电压。

        2. layout对于电源非常重要,你必须采用PCB layout, 并且紧凑布局,功率回路尽量小。面包版洞洞板之类基本上都是很难带载正常的。

        3. 注意sense电阻的layout, 以及建议增加一个小电容尽量靠近sense脚滤波。

  • 你好,我是用洞洞板做的,并且布局很紧凑了,比webench给出PCB板大一点,至于电感我是用环形电感,因为材料有限,饱和电流只有3.0A所以我用大一些的电感来弥补不足,55uh,我现在加多一个小电容在sense 试一试,谢谢

  • Hi

         洞洞板基本上是没法带载的,你需要采用正规PCB, layout