这边PMID、SYS、LS/LDO、VINLS这几个引脚不懂什么意思,datasheet上没有详细的解释。请问遇到这种情况应该去哪查看相关资料。LS/LDO和VINLS从内部框图来看,是通过一个FET相连的,不知具体是什么关系?PMID、SYS反复参阅大概知道都是输出电压的,但不知道有何区别,适用于什么场合?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. datasheet里, pin脚定义里有详细的解释。不知道你的datasheet是不是最新的官方版。
2.结合结构框图,也可以理解这些脚的功能和你的其他问题。
Hi
PMID: High Side Bypass Connection 输入电压出来的供电输出。
SYS,降压转换的输出,可以提供供电到系统System.
LS/LDO、VINLS , 这个只是一个Load swither 的输入和输出。
以PMID为例:
| High Side Bypass Connection. Connect at least 10-µF ceramic capacitor (at least 3µF of ceramic capacitance with DC bias derating) from PMID to GND as close to the PMID and GND pins as possible. |
确实感觉读不懂这个引脚用来做什么,后面只说要接一个常见的去耦电容。