使用TPS63031芯片,测试条件:4.2V输入,3.3V输出。电子负载CC模式最大能调到300mA左右,调不到手册上说的800mA
希望能跟大家讨论讨论,还请不吝赐教,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用TPS63031芯片,测试条件:4.2V输入,3.3V输出。电子负载CC模式最大能调到300mA左右,调不到手册上说的800mA
希望能跟大家讨论讨论,还请不吝赐教,谢谢!
建议换成CR或者CV模式,这是稳压源,保险丝的话你可以并联两个,以实现800mA不熔断
你好,
你的PTC看一看阻抗,有没有可能PTC的阻抗不正常(太大)影响了结果,去掉PTC试试,谢谢。
你好,
你可以测一下保险丝两端的电压,可能虽然没有断路但在超过500mA时电阻变大,建议换大规格的保险丝。