Other Parts Discussed in Thread: TPS40170
整个方案供电是24V5A直流电源输入, 然后通过TPS40170芯片转换为12V@4.5A输出,但是整个板子的功耗是12V@10A左右, 一片TPS40170芯片输出的12V@4.5A不够功耗,所以想能不能用两片TPS40170输出的12V@4.5A并联起来提供12V@9A的电流。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS40170
整个方案供电是24V5A直流电源输入, 然后通过TPS40170芯片转换为12V@4.5A输出,但是整个板子的功耗是12V@10A左右, 一片TPS40170芯片输出的12V@4.5A不够功耗,所以想能不能用两片TPS40170输出的12V@4.5A并联起来提供12V@9A的电流。
Hi
TPS40170外置MOS,直接坐到9A输出没有问题。
不建议采用2个芯片并联输出,建议参照在线仿真webench得到的电路修改,让其直接输出9A.
谢谢Johnsin Tao的解答, 是这样的,我查找过TI的相关参考,有一个参考电路是19~32v输入,输出8A的。但是我这边设计有一个需求,就是一个21V的UPS电源需要为系统供电, 假如我采用了19~32V电压输入的参考设计,UPS电源给电路供电就有问题了。但是如果我采用12~24V电压输入,4.5A电流输出,UPS电源就可以为系统供电了,所以我才会问这个问题。有没有12V~24V电压输入,9A电流左右输出的参考电路。
Hi
按照你的要求,用在线仿真webench就可以得到参考电路,软件在TPS40170官网上。