今天用UCC28180做了一块300W的PFC,在加载过程中输出电压逐渐降低,调整了电压补偿有改善但还是不理想,带到100W负载时395V电压降至370V,ISENSE目前为0.03R,电感量为650uH(PQ3535磁芯绕70T)。请问该如何调整,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
今天用UCC28180做了一块300W的PFC,在加载过程中输出电压逐渐降低,调整了电压补偿有改善但还是不理想,带到100W负载时395V电压降至370V,ISENSE目前为0.03R,电感量为650uH(PQ3535磁芯绕70T)。请问该如何调整,谢谢。
1,直流增益太小了,这一点从调整电压补偿有改善能佐证。输出阻抗等于R_OL/(1+GH),--- R_OL为开环阻抗,由主电路决定,GH为闭环传递函数。因此你需要提高GH(f=0),即提高直流增益。
2. 电压检测Vout和GND是否跟FB电阻的地等电位。