你好,我想问一下我使用TPS76833,想在PG端加一个状态指示灯LED,那IC正常情况下PG端输出的电压是多少?IC不正常是不是输出电压为0?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我想问一下我使用TPS76833,想在PG端加一个状态指示灯LED,那IC正常情况下PG端输出的电压是多少?IC不正常是不是输出电压为0?
Hi
PG 是内部MOS结构,电流推荐最大也就1mA多一些,如果输出电压较低,可能就零点几个mA/
如果你可以接受这个电流的LED,当然没有问题。
PGOOD在输出电压正常时, MOS不导通,PG电压就是输出电压。 当输出电压偏低,MOS导通,可以用一个电阻+LED灯替代250kohm的电阻。此时PGOOD输出为0V, 电阻+LED的总电压就是此时偏低的输出电压。