This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610为:6串(18650)充电,多次烧坏IC。充电电压设定25.2V,充电电流2A。电源适配器28V/2A



大家好!

        BQ24610为:6串(18650)充电,多次烧坏IC。充电电压设定25.2V,充电电流2A。电源适配器28V/2A

打样板时已有发生,多次认为是输入源的问题。调整了输入源加了28V稳压管加了RC,还有发生BQ24610烧坏击穿。请协助分析,谢谢!

附件原理图。

BQ24610为6串充电.pdf
  • HI

          采用28V输入,确实已经到达推荐输入的极限,容易出现输入源过压的情况,特别是你的充电电流还比较大。

          确认duty上没有问题,建议将输入做到27V, 至少可以在测试中这样做。稳压管改为28V的TVS管,功率大一些。输入走线宽一些,避免寄生电感。如果输入走先较长,输入端建议增加一个220uF的电容,用于消除导线寄生电感产生的Spike.

          输入电源启动,注意是软开关,避免输出有过冲。