This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133不充电,SW脚没有波形输出

Other Parts Discussed in Thread: BQ24133

TI,
  目前第一次用BQ24133, 始终充不了电。
电路为:
 

量到各管脚电压为:

1 ,24脚 (SW)12.4V
2 ,3脚(PVCC)  15V
4 脚(AVCC) 15V 

5脚 (ACN)  14.1V
6脚(ACP)14.1
7脚(CM) 14.2V
8脚(ACDRV) 16.3V
9脚(STAT) 0.6V

10脚(TS) 2.8V
11脚(TTC) 0.2V
12脚(VREF) 3.9V
13脚(ISET) 0.63V
14脚(CELL) 3.9V(3节锂电池串连)

15脚(SRN) 12.4V

16脚(SRP) 12.4V
17脚(ACSET) 1.3V
18脚(OVPSET) 1.5V
19脚(BATDRV) 14.1V
20脚(REGN) 0.2V
21脚(BTST) 12V

从电压上看VREF  REGN都不对 ,不清楚到底哪里出问题了。
电路上,SYSTEM那里接了一个2200uF的电解电容,不知道是否影响到电路的正常工作