+12V转-12V
4700PF实际改为300nF,11.3K实际改为13K,1N5819改为SS34丝印贴片二极管。此时已有输出,为-12.6V,且已带负载工作过。
而后约么一天左右PCB板子再通电,检测不到-12V电压。此时输出为基本为0,10mV级别,芯片无发烫现象,测得电源脚和GND电阻大约250欧,1脚PH电压9.2V
更换BOOT启动电容后,此时电压有异常,在0.8V左右100mV飘忽不定,芯片发烫。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
+12V转-12V
4700PF实际改为300nF,11.3K实际改为13K,1N5819改为SS34丝印贴片二极管。此时已有输出,为-12.6V,且已带负载工作过。
而后约么一天左右PCB板子再通电,检测不到-12V电压。此时输出为基本为0,10mV级别,芯片无发烫现象,测得电源脚和GND电阻大约250欧,1脚PH电压9.2V
更换BOOT启动电容后,此时电压有异常,在0.8V左右100mV飘忽不定,芯片发烫。
Hi
如果芯片Vin与GND之间阻抗偏低(到250ohm左右),芯片已经烧掉了,再通电发热是必然。
如果确认芯片是烧掉了,建议你回忆一下通电操作中是否有异常? 另外ESD也是有可能的。
另外电路上输入Vin12V到输出-12V之间必须有稳压电容。