This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM22671工作频率问题



请教一下,我焊接了5块22671的电源板,用的元件都是一样的,频率调节电阻用的都是1%的100k,虽然电源都能正常工作,但是每个板子的工作频率都不一样,范围从350k到410k都有,差异是比较大的,我想问一下这个是否正常?因为频率控制不好我怕影响外部负载引起共振效应。

  • Hi

         按照datasheet参数表,当内部震荡频率是500kHz时,时间频率的tolerance分布在400~600kHz, 存在+/-20%的范围差异,所以即便是外接电阻控制频率,也同样存在很大的频率tolerance,故范围分布350k到410kHz是正常的。

         这个频率分布通常不会与负载产生共振现象。

         按照您的频率设计,可以外接滑动变阻器调节频率来验证,测试按照20%的tolerance频率范围内,输出是否存在异常。