请问TI的员工,该芯片有一个参数V(UVLO)是用来干嘛的?LS_LDO_OCP fault又是什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
见datasheet对V(uvlo)的规格定义: V(UVLO)即input under-voltage, 输入欠压
具体看输入电压Vin欠压保护(UVLO)描述:The input under-voltage status indication is used to notify the host or other device when the input voltage falls below a desired threshold. When VIN < VUVLO, after the deglitch time tDGL_UVLO, a UVLO fault is determined to exist. During the VIN UVLO fault, the device sends a single 128-µs pulse on INT, and the STAT and FAULT bits are updated over I 2C. The FAULT bits are not cleared until they are read in from I 2C after the UVLO condition no longer exists.
OCP 即Over current protection, 这个是Load swither 限流保护。