This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3307-18问题咨询

Other Parts Discussed in Thread: TPS62040, TPS3307

1、在3307的资料中看到3307-18的VDD使用1.8v供电(SGLS140A),这个是不是写错了?3307是2-6v供电范围。

2、slva056a.pdf中推荐对于3307-18的SENSE3的电阻选择,“The sum of both resistors should be about 1 M”,是否是必须的?如果选择了5V接入SENSE3来检测,使用电阻为R1=33K和R2=18K是否可以?

3、VDD旁边的电容是否必须接?如果是TPS62040输出的3.3V给3307供电,这个电容没有接,是否会引起复位?

4、目前发现做的板子偶尔有一块板子极小概率的复位。

  • 你好,

    第一个问题:针对TPS3307系列推荐使用在2~6V供电,SGLS140A中示例的是TPS3307-18,也可以在1.8V工作。

    第二个问题:不是必需的,电阻选大有个好处就是降低功耗。

    第三个问题:强烈建议你给TPS3307 VDD引脚加上旁路电容,特别是采用DC/DC供电时,旁路电容不要省略,可保证复位可靠性。

  • 1. 3307-18-EP是增强型的,与3307-18是同一源,但已做部分优化。对于3307-18的VDD使用1.8V供电,产品线回复如下:

    I do not recommend operating the TPS3307-18 at 1.8V on VDD. The device is not fully characterized for VDD=1.8V and therefore performance is not guaranteed. I recommend operating VDD from the 3.3V rail which is also sensesd (or some other voltage rail within the recommended range specified in the datasheet)

    3. VDD的旁路电容:最好是接上0.1uF的陶瓷电容,这个电容的作用:输入信号SENSE2中的高频噪声作为滤除对象,把所携带的高频杂波滤除(SENSE1最好也加上一旁路电容),以避免TPS3307-18检测到低电平信号,而引起3307的复位。