1、在3307的资料中看到3307-18的VDD使用1.8v供电(SGLS140A),这个是不是写错了?3307是2-6v供电范围。
2、slva056a.pdf中推荐对于3307-18的SENSE3的电阻选择,“The sum of both resistors should be about 1 M”,是否是必须的?如果选择了5V接入SENSE3来检测,使用电阻为R1=33K和R2=18K是否可以?
3、VDD旁边的电容是否必须接?如果是TPS62040输出的3.3V给3307供电,这个电容没有接,是否会引起复位?
4、目前发现做的板子偶尔有一块板子极小概率的复位。