This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92640没有电流输出,怎么办?



情况描述:

上电后BUCK电路的上管那个MOS的G极和S极就和地导通了(断电不导通,测试是通过芯片导通的);

下管那个MOS管的G极有一个方波信号,频率有3MHz;

用万用表测SW节点和地是导通的,因此电感上没有电流。

我的输入是48V,要输出3A。

设置的欠压保护是40V;过压保护是60V;开关频率设置500KHz

测试各引脚电压为:

VIN:  47.6V  ;

UDIM:2V;

VREF:3.05V

IADJ:1.75V;

COMP:2.8V;

BOOT:10V;

VCC:8V;

RON,VOUT,HG,SW,CS,GND都是0V.

LG是一个占空比为2/3。周期为320ns左右的方波信号。

上电一段时间后芯片会发烫。