最近做了一个BQ77904+BQ24130的充放电电路板,测试过程中发现如下问题:
1、BQ77904在放电过程中,当UV、OCD1、OCD2、SCD保护触发之后,不能恢复,只能通过拔掉电池再上电池才能恢复,检查之后我将RGS_CHG 更换为3.3M欧姆依然不能恢复。
2、对于BQ77904的CCFG这个PIN,规格书中有Note that the bq77904 should be configured in 5S mode as this results in a permanent UV fault.那么当前板子用的是3S的充放电,我将CCFG连接到DVSS是否有问题。
3、我使用的BQ24130充电配快充的时候,按2A的分压电阻配置ISET1,但实际过程中始终无法达到2A充电,只有1A,当配置为慢充的时候,按200mA配置ISET2而充电电流就是设置的200mA.为什么当前方案快充不能达到2A?
4、当前电池充电过程中,后期电流会逐渐降低直到充电电流不在变化,但是STAT的状态一直不会变化,导致与之连接的指示灯(充电指示灯)不能熄灭。当前使用的是+5V通过DC-DC到13.16V给BQ24130,BQ24130的内部DC-DC降压之后输出12.53给3S的锂电池充电。
以上问题已困扰了一段时间,特别是问题1,还请及时回复,谢谢!
附上相关部分电路图: